DNP3

Pulse Control Example

This example demonstrates how the On Time, Off Time and Pulse Count properties can be used to specify how many pulses are triggered by a single control action.

The first pulse within any DNP3 pulse control starts as soon as the execution of that control commences.

Example:

A DNP3 Pulse Action is configured as follows:

Pulse Count: 3
On Time: 1S (one second)
Off Time: 2S (two seconds).

This configuration means that for each control operation, three 1-second pulses are generated, each two seconds apart.


Disclaimer

Geo SCADA Expert 2021