DNP3

Specify When the Slave Outstation is to Invalidate its Pair of Session Keys

To maintain security, the DNP3 master changes the Slave outstation’s current set of Session Keys whenever the DNP3 master’s change interval or change count is reached (whichever is the shorter). The DNP3 master also changes the Session Keys after detecting any communications failure.

Use the fields within the Session Keys section of the Security tab to specify how long the Slave outstation (Geo SCADA Expert) should wait before invalidating its pair of Session Keys, should an expected Session Key Change not occur.

Ideally, the values that you specify in these fields should be twice the size of the values set in the DNP3 master. This will mean that Geo SCADA Expert does not invalidate its Session Keys unnecessarily, should a Session Key Change be delayed when the system is exceptionally busy. (Should the Slave outstation invalidate its Session Keys, it will be unable to process any further critical requests. This will result in authentication failures, causing the DNP3 master to issue a new set of Session Keys once the DNP3 master’s Maximum Error Count has been exceeded.)


Disclaimer

Geo SCADA Expert 2021