DNP3

Transfer Data Between a Configuration Tool and Three Flow Computers

This example demonstrates how Geo SCADA Expert might be configured in order for it to transfer data between a Flow Computer Configuration Tool and three Flow Computers.

Example:

A Geo SCADA Expert system is used to transfer data between a Flow Computer Configuration Tool and three Flow Computers. In order to facilitate this, a VT Service Port Master is configured in the Geo SCADA Expert database, along with three Virtual Terminals—one terminal for each outstation port (A, B, and C) that is being used to route the communications. Each Virtual Terminal Number configured in the database is used to uniquely identify one of the outstation ports.

The same Geo SCADA Expert system is also used to transfer data between two DEC VT Terminals. In order to facilitate this, a second VT Service Port Master is configured in the Geo SCADA Expert database, along with a fourth Virtual Terminal. This Virtual Terminal is for outstation port D—the port that is being used to route the communications to the DEC VT Terminal.

The ‘Master Port’ field on the Virtual Terminal Form is used to define which VT Service Port Master is associated with each Virtual Terminal.

Further Information

Configure a DNP3 VT Service Port Master.

Configure a DNP3 Virtual Terminal.

Define the Virtual Terminal Support requirements using the DNP3 master Outstation Form: see Configure Virtual Terminal Support.


Disclaimer

Geo SCADA Expert 2021