DNP3

Use Persistence to Stop Fleeting Changes in Value from Changing a Point State

You can use Persistence to prevent momentary changes in point value from changing the state of a point. When used, persistence stops the driver from processing the fleeting changes in point state and reporting those fleeting changes to the server. This stops Geo SCADA Expert from raising change of state alarms and logging change of state events when a point value is fluctuating.

You specify the type of persistence using a point’s Persistence Type field. You use this field in conjunction with the Persistence Duration fields, which define the required amount of time before a change in point value is recorded as a change in point state. The persistence fields are on the <Point Type> tab of the Point Form.

Use the Persistence Type field to specify one of the following:

Persistence delays the recording of a change in state, not the recording of a change in value. If a point is also configured to use Significant Change and a change in value exceeds the Significant Change Deadband, the value of the point will be updated immediately, although the state will not have changed at that stage. Any change in state will only be recorded, along with the point’s current value at that time, once the Persistence Duration has elapsed. (For an example that demonstrates this, see Examples of Persistence with an Analog Point.)

With a Persistence Type other than ‘None’, use the point’s Persistence Duration fields to specify the amount of time during which a change in state has to persist, before that change in state is recorded:

With binary points, a Persistence Duration field exists for each point state.

With analog points, a Persistence Duration field exists for each state limit. (With the DNP3 driver, persistence does not apply when an analog point's value travels into the Invalid state, as that state is reported immediately.)

For each change in state that is to persist before it is recorded, use the relevant Persistence Duration field to specify the required time period. Enter the required interval in the OPC Time Format. You can enter the value directly in the field, or use the Interval window (accessed via the field's browse button) to specify the required value. (Leave a Persistence Duration field at the default of 0 for any state changes that are to be recorded immediately.)


Disclaimer

Geo SCADA Expert 2021