Configure the Control/Status Properties

Use the fields within the Control/Status section of the SCADAPack tab on the Outstation form to configure the Control/Status properties.

The availability of the properties in this section of the tab vary depending on the outstation type. You select the Outstation Type from the Outstation Type tab (see Specify the Outstation Type). With some outstation types, the settings of some of the properties are fixed; such properties appear 'grayed out' on the configuration Form. This table indicates which Control/Status properties each type of outstation supports:

Control/Status Property Supported Outstation Types
LED Power Always On SCADAPack 312E, 313E, 314E, 330E, 333E, 334E, 337E, 350E, 357E, 530E, 535E
Vision Power Pin Enabled SCADAPack 330E ,333E, 334E, 337E, 350E, 357E, 530E, 535E
VLOOP Output Select SCADAPack 350E, 357E
24 DC/DC Converter Control SCADAPack 350E, 357E

 


Disclaimer

Geo SCADA Expert 2021