Configure Pulse Properties

Use the fields at the top of the Pulse Action tab to define the general properties of DNP3 SCADAPack Pulse Action (NULL) or DNP3 SCADAPack Pulse Action (Trip-Close) points.

The first three fields are common to Pulse Actions on the DNP3 driver—for information, see Configure Pulse Properties in the Geo SCADA Expert Guide to the DNP3 Driver.

For information on the Interlock fields, see Configure an Output Point or Pulse Action’s Interlock Properties.

Fields that are specific to DNP3 SCADAPack Pulse Actions are summarized below.


Disclaimer

Geo SCADA Expert 2021