Configure TCP Service Port Properties

TCP Service Ports permit SCADAPack E outstations to provide virtual serial ports over a TCP/IP connection. For a port to be used in this way, the port’s Function has to be set to TCP Service (see Configure the Properties of the Individual Ports). You can configure more than one SCADAPack E outstation port to have this function, so providing multiple virtual serial ports. For a SCADAPack E outstation to support TCP Service Port connections from multiple TCP/IP hosts, for example, each host has to connect to a different port (as only one TCP connection per virtual serial port is permitted).

Many Geo SCADA Expert drivers can communicate with serial devices over a TCP/IP link using a TCP Service Port.

Use the fields within the TCP Service Ports section of the SCADAPack TCP/IP tab to define the properties that the SCADAPack E outstation uses for TCP Service Port connections:

A SCADAPack E outstation can also be configured as a TCP Services Port Client. In this mode, the outstation establishes the TCP connection to a TCP Services Port Server. See the SCADAPack E TCP/IP Technical User and Reference Manual for further information.


Disclaimer

Geo SCADA Expert 2021