Configure the Trend Retrieval Properties

This section only applies if the outstation samples input or derived point data for particular trends (see Configuring DNP3 SCADAPack E Trend Sampler Functionality).

When an outstation samples any counter, analog input, binary input, or derived analog or binary data, it stores the values that fulfill the sample criteria locally at the outstation. Use the fields within the Trend Retrieval section of the SCADAPack tab to specify when that data is retrieved for use in Geo SCADA Expert:

With a DNP3 SCADAPack E PSTN outstation, Geo SCADA Expert retrieves any stored sampled data values from the outstation whenever it is in communications with that outstation.


Disclaimer

Geo SCADA Expert 2021