Limitations and Restrictions

This section summarizes the limitations and restrictions that need to be taken into account when configuring a Profile and associating that Profile with a DNP3 SCADAPack point or pulse action.

With standard (‘core’) Time Profiles, the specified Profile:

Further Information

Configuring Standard Time Profiles: see Configuring Time Profiles in the Geo SCADA Expert Guide to Core Configuration.

With daily DNP3 SCADAPack Profiles, the specified Profile:

(The profiles for a binary point or pulse action can only contain the profile values 0 and 1. The profiles for a counter point can only contain profile values greater than or equal to 0. Both ViewX and the Automation Interface will reject any attempt to enter values that are deemed to be invalid (see Manually Edit the Vectors on a DNP3 SCADAPack Profile).)

If a Daily (DNP3 SCADAPack) profile does not have a value specified at midnight at the start of the day, Geo SCADA Expert will assume the starting value to be that of the previous day’s last profile value. (The previous day’s profile being that specified for the previous day in the Profiles section of the Point Form.)

 

Further Information

Configuring DNP3 SCADAPack Profiles.


Disclaimer

Geo SCADA Expert 2021