Specify any Point Mapping

This section only applies to DNP3 SCADAPack points that have their Point Type set to Physical Input or Physical Output (see Configure Common Properties of DNP3 SCADAPack Points). (For other Point Types, the Mapping tab is disabled.)

Use the fields on the Mapping tab of the DNP3 SCADAPack Point Form to Specify Whether Point Mapping is Used to define the source and location of the point data. When mapping is used, the fields on the tab vary, depending on the type of point and the device to which point data is being mapped.

DNP3 SCADAPack Trip-Close Pulse Actions have two Mapping tabs—one for each pulse action. Ensure that the relevant properties are configured on each of these tabs.


Disclaimer

Geo SCADA Expert 2021