Specify the Profile Type

Use the Profile Type field toward the bottom of the SCADAPack tab to specify the type of Profile that is used by the outstation’s points.

NOTICE

UNEXPECTED BEHAVIOR OF APPLICATION

Take great care if you need to change an existing outstation’s Profile Type at some future date from Standard to Daily, or vice versa. Changing an outstation’s Profile Type will remove the existing Profile entries from the configuration Forms of the points on that outstation. (As that type of Profile would no longer be deemed to be valid.)

Ensure that you update each point’s configuration as required.

Failure to follow these instructions can result in unexpected configuration changes.

Select the type of Profile that is appropriate to your way of working. Choose from:


Disclaimer

Geo SCADA Expert 2021