Specify the Properties of a File in a SCADAPack E Outstation’s Configuration

Use the Properties button on the Configuration Setup Window to edit the properties of a file in the SCADAPack E outstation’s configuration. The Properties window is also displayed when you add a file to the DNP3 SCADAPack E outstation’s configurations (see Add a File to a SCADAPack E Outstation’s Configuration).

The Properties window is not available for RTU Configuration files that are temporarily generated using the Generate button on the Configuration Setup window (see Generate Configuration and Profile Files for Diagnostic Purposes).


Disclaimer

Geo SCADA Expert 2021