Tune Limits Alarm

Associated with: DNP3 SCADAPack Analog points and DNP3 SCADAPack Counter points.

This status attribute indicates an alarm state if Geo SCADA Expert’s last attempt to download the point’s alarm limits configuration to the SCADAPack E outstation was unsuccessful. Geo SCADA Expert attempts to download such configuration in response to a Tune Alarm Limits pick action request.

For example, a download would be unsuccessful if communications were lost during the download, or an attempt was made to tune the limits of a point for which configuration did not yet exist in the outstation.

Possible states: Displays one of the Standard Alarm States.


Disclaimer

Geo SCADA Expert 2021