UpdateFile

Associated with: DNP3 SCADAPack E outstations and DNP3 SCADAPack Remote E outstations

Security permission required to access this method: Configure

Use this method to replace a file that exists in a DNP3 SCADAPack E outstation in the Geo SCADA Expert database, with a new copy of the file.

This method is the equivalent of updating a file via the Update button on the Configuration Setup window (see Update a File in a SCADAPack E Outstation’s Configuration).

Arguments:


Disclaimer

Geo SCADA Expert 2021