The outstation sets on advanced drivers support a combination of these actions:
- Cancel Promoted Dial Out
- Disable Set
- Disable Switching—(Shared or Switched sets only)
- Display Outstations
- Enable Set
- Enable Switching—(Shared or Switched sets only)
- One Shot
- Promote Dial Out
- Release Exclusive Control—(Systems on which Exclusive Control is enabled)
- Switch Line—(Shared or Switched sets only)
- Take Complete Exclusive Control—(Systems on which Exclusive Control is enabled)
- Take Partial Exclusive Control—(Systems on which Exclusive Control is enabled).
                            
Further Information
‘Core’ pick actions that are common to many database items: see Object Menu Options.
For information on any outstation set-specific actions that are not listed above, see the relevant driver guide.