Alarm Limits

Associated with: Analog and Counter-type points for which alarm limits are currently tuned and/or the Multiple Alarm Limits feature is enabled.

This status attribute is only displayed for points on which:

The attribute lists the following:

If multiple alarm limits are enabled and the alarm limits are also tuned, tuning takes precedence over multiple alarm limits.

Also see M/S Alarm Limits.


Disclaimer

Geo SCADA Expert 2021