Mark

If the channel and communications equipment are configured to use Mark Parity, the communications equipment expects the Parity bit to be set to 1 in all data transmissions:

However, in some instances, the ‘receiving’ communications equipment is not expected to reply even if the message was received correctly. In these situations, further diagnostics of the communications network and device are required.


Disclaimer

Geo SCADA Expert 2021