Outgoing Call Quality Factor

Associated with: PSTN channels that are chosen due to their higher quality factor, rather than the fewest total calls

This status attribute is only displayed if:

The status attribute indicates the channel’s current call quality factor and the date and time at which that quality factor was last updated (the date and time of the last outgoing call via the channel).

Example:

5 last updated at 06/Jul/2009 16:25:04.832


Disclaimer

Geo SCADA Expert 2021