Put Aside Last Updated

Associated with: Points for which a local Override is currently in force

This status attribute displays the last update time of the point data that was ‘put aside’ when the current local Override came into force.

Use the attribute in conjunction with the other Put Aside status attributes (such as Put Aside State and Put Aside Value) to ascertain further information about the point data that was ‘put aside’.


Disclaimer

Geo SCADA Expert 2021