State

Associated with: Driver items other than outstation sets, points, and pulse actions

(Points have several ‘State’ status attributes, including Current State and Previous State.)

The State status attribute indicates the present state of the item. The possible values vary, depending on the type of item.

A server might be in one of these states:

A channel on a simple driver might be in one of these states:

A scanner might be in one of these states:

For more information on the checks to undertake should a scanner on your system not be in a healthy state, see Troubleshooting in the Geo SCADA Expert Guide to Simple Drivers.

A Slave source might be in one of these states:

A channel on an advanced driver might be in one of these states:

An outstation might be in one of these states:

For more information on the checks to undertake should an outstation on your system not be in a healthy state, see Troubleshooting in the Geo SCADA Expert Guide to Advanced Drivers. The section includes a list of diagnostic messages that might be displayed should Geo SCADA Expert detect a communications problem.

A Slave outstation might be in one of these states:


Disclaimer

Geo SCADA Expert 2021