Define the Data Retrieval Intervals

The configuration Forms of EtherNet/IP Outstations include an EtherNet/IP tab. Use the Retrieval Intervals section of the EtherNet/IP tab to determine how often the driver polls an Allen-Bradley controller to retrieve its point data:

To define which of the eight Normal/Promoted intervals is used for a particular point, use the Retrieval Interval field on the <Point> tab of the corresponding EtherNet/IP Point Form (see Configure Common Point Properties).

Example:

An analog point on an EtherNet/IP Outstation has this configuration:
Retrieval Interval: 5

The EtherNet/IP Outstation includes this configuration:
Normal Retrieval Interval 5: 8S
Promoted Retrieval Interval 5: 4S
The Promote when Displaying Points check box is selected.

Geo SCADA Expert scans the controller that the EtherNet/IP Outstation represents every eight seconds for the analog point data.

A Mimic that contains a point from the controller is displayed on one of the ViewX workstations.

While the Mimic is on display, scanning of the controller is promoted. While scanning is promoted, Geo SCADA Expert scans the controller at four-second intervals for the analog point data.


Disclaimer

Geo SCADA Expert 2021