Minimum Configuration - Outstation

This topic relates to outstations on the EtherNet/IP driver. The EtherNet/IP driver supports Direct Outstations and Shared Outstations.

When you add an item to the database, various properties on the item's configuration Form are assigned a value automatically. These default values are assigned on creation of the database item, to help reduce the amount of manual configuration that is required. As such, you only need configure a subset of the properties that exist on an item's configuration Form. Typically, the properties you have to configure include:

For an outstation on this driver to be capable of functioning in Geo SCADA Expert, as a minimum you have to configure the following:

With a Shared Outstation, you also have to configured the Shared properties, located on the Shared tab.

Also ensure that the outstation and the database items on which it depends are In Service, and have saved, valid configuration. This will produce an outstation that is capable of functioning using the default configuration settings.


Disclaimer

Geo SCADA Expert 2021