Define the Point Scaling

Use the fields in the Scaling section of the Analog Point Form to specify the type and range of the raw input signals, so that they can be suitably converted into floating-point engineering values for use in the Geo SCADA Expert database.

Conversely, if the point is configured as an output point, use this Scaling section to perform a similar conversion on any output signals. Geo SCADA Expert uses the conversion calculation to produce a raw data value that is sent to plant.

There are two levels of scaling that can be applied to an EtherNet/IP Analog point. The first level is scaling a raw value into an engineering value using linear interpolation. This level of scaling is only applied when it is enabled. The second level of scaling is where the Multiplier and the Offset values are applied. This second level of scaling is always applied.


Disclaimer

Geo SCADA Expert 2021