Accessing the Expression Window

You will need to use the Expression Window during the configuration of many different types of database item, including Mimics and Trends. The features that are provided by the Expression window will vary according to the type of item that you are configuring. For example, the Expression window for a Data Grid has slightly different settings than the Expression window for a Mimic.

You can use the Expression window to enter an expression. The expression defines the value that will be calculated by Geo SCADA Expert.

To access the Expression window:

The Expression window is not the only interface that you can use to enter an expression. Some fields provide similar functionality to the Expression window (see Expression Fields) and on Mimics and Data Grids you can also use the Expression Flowchart to create IIF statements.


Disclaimer

Geo SCADA Expert 2021