COS

The COS function is a mathematical function that returns the Cosine (radians) of a number. The COS function returns a real value.

Function Name

COS

Description

Returns the Cosine (radians) of a number.

Arguments

COS(INTEGER OR REAL)

The value can be an integer or a real floating value—see Number (Integer or Real).

Returns

The Cosine (radians) of a number. This is of the same type as the input (INTEGER or REAL).

Example:

COS( PI() )

The output is -1.


Disclaimer

Geo SCADA Expert 2021