FIX

The FIX function is a mathematical function that removes the fractional part of a real number and returns the result as an integer value.

Function Name

FIX

Description

Removes the fractional part of a real number and returns the result as an integer value.

Arguments

FIX(INTEGER or REAL)

For more information, see Number (Integer or Real).

Returns

INTEGER

The integer value that is numerically equal to the integer part of the input value.

Example:

FIX(1.735)

The output is 1.

FIX (8.5)

The output is 8

FIX(-8.6)

The output is -8.


Disclaimer

Geo SCADA Expert 2021