Configuring ICMP Points in Geo SCADA Expert

For Geo SCADA Expert can use ICMP to detect whether network-connected devices are reachable. To do this, the ICMP Driver has to be installed and running on the Geo SCADA Expert servers on your system.

You also need to configure one ICMP Digital Point in the Geo SCADA Expert database for each network-connected device that the driver is to monitor using ICMP (see Configuring ICMP Digital Points).

You need to be aware of which optional features are required for each ICMP Point. These features include:

You can also use other core Geo SCADA Expert features with ICMP Points, including Lists, Actions and Mimics. For actions that are specific to the ICMP driver, see Using ICMP Specific Actions. For further information on actions and for details on Lists and Mimics, see the core documentation.


Disclaimer

Geo SCADA Expert 2021