Define the File Transfer Parameters

The IEC 60870-5 protocol allows a variety of files to be transferred between the SCADA master station and an IEC 60870-5 outstation.

Use this field in the IEC 60870-5 section of the Server Configuration Tool to specify the parameters for such file transfers:


Disclaimer

Geo SCADA Expert 2021