Minimum Configuration

For an IEC 60870-5 Direct Outstation to become functional (online), you need to configure these properties:

These are the minimum requirements for configuring a functional IEC 60870-5 direct outstation.

For an IEC 60870-5 Shared Outstation to become functional (online) you need to configure the above properties, plus the properties on the Shared tab.

For an IEC 60870-5 Logical Outstation to become functional (online), you need to configure these properties:

These are the minimum requirements for configuring a functional IEC 60870-5 logical outstation.

With either type of outstation, you also need to put the outstation In Service and save the configuration. This will result in a functional IEC 60870-5 outstation that uses the default configuration settings.


Disclaimer

Geo SCADA Expert 2021