ASDU

An Application Service Data Unit (ASDU) is a block of data that is sent from the Controlling Station (SCADA master) to an outstation or other device (such as Geo SCADA Expert), or vice versa, using the IEC 60870-5 protocol.


Disclaimer

Geo SCADA Expert 2021