Configure Polling

If you intend to use polling to request data, you need to enable and complete the Polling sections on the relevant IEC 61850 configuration Forms. Use the fields within the Polling section to specify polling that Geo SCADA Expert is to apply to that particular point.

To configure the polling requirements complete the following fields:

 


Disclaimer

Geo SCADA Expert 2021