Configure the Control Options

The Control Options is available in the IEC 61850 Analog and Digital Control Point Forms. To understand how these options effect the way the control object behaves refer to the state machine diagrams in Controls with Normal Security and Controls with Enhanced Security sections.

The following properties can be configured manually but are automatically set as shown below during point creation:


Disclaimer

Geo SCADA Expert 2021