Control Point Data Types

IEC 61850 defines many controllable data classes, Geo SCADA Expert encapsulates them all as Analog or Digital Control points. The table below shows the mapping of IEC 61850 Data Class and Data Type to MMS Data Type and the type of control used.

Data Class IEC 61850 Data Type MMS Data Type Control Type
Controllable single point (SPC) BOOLEAN Boolean Digital
Controllable double point (DPC) BOOLEAN Boolean Digital
Controllable integer status (INC) INT32 Integer Analog
Controllable enumerated status (ENC) ENUM Integer Analog
Binary controlled step position information (BSC) CODED ENUM Bit-string Analog
Integer controlled step position information (ISC) INT8 Integer Analog
Controllable analogue process value (APC) {INT32;FLOAT32;} {Integer;Unsigned;} Analog
Binary controlled analog process value (BAC) CODED ENUM Bit-string Analog

Disclaimer

Geo SCADA Expert 2021