Controlling Station

A Controlling Station is the SCADA master station at which telecontrol of the Controlled Station (outstations) is performed. On a Geo SCADA Expert system that is running the IEC 61850 driver, the Geo SCADA Expert server is the controlling station.

Throughout this guide, the controlling station is referred to as the Geo SCADA Expert server.


Disclaimer

Geo SCADA Expert 2021