Kingfisher Outstation Communicating Directly with Geo SCADA Expert

Using the Kingfisher protocol, the Geo SCADA Expert system can act as a Kingfisher Master and poll a Kingfisher outstation.

For this scenario, within Geo SCADA Expert you need to configure a Kingfisher Channel (as appropriate to the type of communications being used), a Kingfisher Outstation Set, and a Kingfisher Outstation. You also need to configure points in the database, to correspond to the points in the Kingfisher outstation. For further information, see Kingfisher Master Configuration.

Example:

In the diagram below, Geo SCADA Expert is using the Kingfisher protocol to communicate with a Kingfisher outstation. The points configured for the Kingfisher outstation in the Geo SCADA Expert database correspond to the points that reside in that outstation.


Disclaimer

Geo SCADA Expert 2021