Scan Duration

Associated with: Kingfisher Direct channels

This status attribute indicates the shortest and longest times taken to complete a scan on a particular channel, along with the average scan completion time on that channel.

If the Reset Statistics pick action has been used to reset the duration, two Scan Duration attributes are displayed. The first displays the scan durations since the last reset; the second displays the scan durations between the previous two resets.

Example:

Minimum 1 seconds, Maximum 5 seconds, Mean 2 seconds


Disclaimer

Geo SCADA Expert 2021