Refresh the Data on a List other than an Alarms List 
            
                
Similarly, while the Events List 
‘Custom’ Lists with complex queries that include, for example, summary functions (SUM) and/or GROUP BY clauses, only update when a Refresh is issued. A Refresh is required if there is no one-to-one correlation between the entries on a List and the Ids or RecordIds that would otherwise identify the records in the Geo SCADA Expert database.
To ‘refresh’ a List with the latest data:
- Right-click on the List.
A context-sensitive menu is displayed. - Select the Refresh Query option.
 
Alternatively, on a ViewX client, you can:
- Press the F5 function key on the keyboard.
 
(Closing and then redisplaying a List also refreshes the data on that List.)