Specify the Properties of the Font used in List Headers

This section only applies to Lists—for information on changing the font properties of the Alarm Banner, see Specify the Properties of the Font used for the Alarm Banner in the Geo SCADA Expert Guide to Alarms.

Use the Header Font section of the Option window’s Lists tab to specify the properties of the font used in List headers:

Once you have confirmed the settings, you will need to close and re-open any Lists that are presently on display, in order for the changes to take effect on those Lists.


Disclaimer

Geo SCADA Expert 2021