Understand Historic Lists

You can Display a Historic List for an individual point that has Historic Logging enabled, or for an individual master station accumulator.

Each Historic List comprises a series of rows and columns, and contains the data that is stored historically in the Geo SCADA Expert database for that particular point or accumulator. Each row comprises the data for an individual historic record. The column headings indicate what the data in each column represents.

Be aware that Geo SCADA Expert supports historic data compression, whereby unnecessary data can be filtered out so that only those entries that are of interest are stored historically. Compression is mainly used to reduce storage requirements for historic data, and is typically used with points on simple drivers rather than advanced drivers. For more information on compressing point data, see Historic Data Compression. For information on compressing accumulator data, see Tabs on Accumulator Forms. There are some updates to which compression settings do not apply—Geo SCADA Expert logs such updates historically regardless of any compression settings (see Point Updates to which Compression Settings do not Apply and see Accumulator Updates to which Historic Data Compression Settings do not Apply). You can determine why Geo SCADA Expert has stored an update historically by looking at the Historic List for the point or accumulator. The column headings for a Historic List are:


Disclaimer

Geo SCADA Expert 2021