ABS

Function Name

ABS

Description

Converts a numerical input into an absolute value. The absolute value is the output and is also a REAL or LREAL value.

Arguments

Input 1 {ANY_NUM}

For more information on the data types for the inputs and outputs, see Data Type Hierarchy.

Returns

Output {Same data type as input}

Example:

Function Block Diagram - ABS:

The ABS function converts values into positive values (if the input is positive, the output is positive; if the input is negative, the output is positive). In this example, the constant input is -324 so the ABS function outputs 324.

ST Program - ABS:

The syntax for an ABS function in an ST Program is:

Output := ABS (Input 1);

Where Output and Input 1 are defined as variables earlier in the ST program. The Input 1 variable represents any type of numerical value.


Disclaimer

Geo SCADA Expert 2021