Declaring a Method in a DATABASE_OBJECT Structure
You can declare methods in a DATABASE_OBJECT structure. This enables you to group methods with database fields.
When you declare a method in a DATABASE_OBJECT structure, if that method has arguments you have to declare those method arguments.
As with defining variables in a DATABASE_OBJECT structure, the main advantages of declaring methods in a DATABASE_OBJECT structure are:
- It reduces the amount of time you have to write the program as you can reference the DATABASE_OBJECT structure rather than the same methods for different database items.
- The methods declared in the DATABASE_OBJECT structure can be used with any items of the same class.
- It makes the program easier to write, read, and understand.
If you declare methods in a DATABASE_OBJECT that is used with an SQL query, you can use the SQL to return methods in the RESULTSET instead of values. For example, you can override any points that have CurrentQuality Desc values of 'Bad'.
Aggregate methods cannot be declared in a DATABASE_OBJECT structure.
To declare methods in a DATABASE_OBJECT structure, you have to use the following format:
TYPE
<database item name>: DATABASE_OBJECT (<class of database item>)
<Method name>: METHOD (<list of argument data types>);
END_DATABASE_OBJECT;
END_TYPE
Where:
<database item name> is the name of the database item to which the methods apply.
DATABASE_OBJECT instructs the program that the methods are part of a database object structure.
(<class of database item>) is the class with which the method is associated. This may be the class for the database item or one of its parent classes. For example, it could be CSCADAPackMPoint for a SCADAPack Modbus point or CDBPoint for all types of point.
<Method name> is the name that you are going to use to identify the method in your program. For methods that are defined in DATABASE_OBJECT structures, you have to enter a name that matches the name of the method in the Geo SCADA Expert database. For example, for an Acknowledge Alarm method, you have to define its name as Accept (as that is the name of the method in the Geo SCADA Expert database).
METHOD instructs the program that the type of value in the DATABASE_OBJECT is a method. (<list of argument data types) specifies the data type of each argument (this section, including the parentheses, is only required if the method has arguments). You have to repeat the <Method name>:METHOD (<list of argument data types>); line for each separate method that is to be included.
END_DATABASE_OBJECT; ends the database object structure definition and END_TYPE ends the type declaration.
Example: 1
TYPE
AlarmConditions: (AlarmNormal, AlarmDisabled, AlarmAcceptedUncleared, AlarmUnacceptedCleared, AlarmUnacceptedUncleared);
END_TYPE
TYPE
AlarmDBOBJ: DATABASE_OBJECT (CDBPoint)
AlarmState:AlarmConditions;
Accept: METHOD;
END_DATABASE_OBJECT;
END_TYPE
In the program, the following ST is used to set the Input1 point so that its UnacknowledgedCleared alarms are acknowledged automatically:
VAR
Input1 AT %O(Input1) :AlarmDBObj;
END_VAR;
PROGRAM
IF(Input1.AlarmState = UnacknowledgedCleared) THEN
Input1.Accept();
END_IF;
END_PROGRAM
This program uses an enumerated data type (see Using Enumerated Data Types to Create Names for State Values). The enumerated data type defines a value named AlarmConditions that has 5 state values. The Geo SCADA Expert Database Schema defines the states as:
- State 0—Normal
- State 1—Disabled
- State 2—AcknowledgedUncleared
- State 3—UnacknowledgedCleared
- State 4—UnacknowledgedUncleared
The encapsulated data type is named and has its state values defined in the first TYPE declaration.
You can use any names for the states in encapsulated data types (they do not have to match the names of states in the Geo SCADA Expert Database Schema).
The second TYPE declaration is used to define the DATABASE_OBJECT structure for the methods. It is named AlarmDBOBJ, and it is set to be a DATABASE_OBJECT that uses the CDBPoint class. The following values and methods are included in the DATABASE_OBJECT:
AlarmState:AlarmConditions;
Accept: METHOD;
The AlarmState value returns a value for the AlarmConditions data type. This means it returns a value that corresponds to one of the AlarmConditions states.
The Accept value defines the method that is used in the program (the Acknowledge method). The name of the Accept value has to match the name of the method as it appears in the Geo SCADA Expert database schema, so in this case it is Accept as the name of the Acknowledge Alarm method is Accept. The METHOD part of the value instructs the program that the value is a method.
In the program, the VAR list contains:
Input1 AT %O(Input1) :AlarmDBObj;
This defines a value (Input1) that is a database item (%O). The Input1 value is associated with the Input1 database item and its values are returned for the AlarmConditions database object structure. This means that the program will use the Input1 item's values that correspond to the values that are specified in the AlarmDBObj structure.
PROGRAM
IF(Input1.AlarmState = UnacknowledgedCleared) THEN Input1.Accept();
END_IF;
END_PROGRAM
This part of the program defines the Logic of the program, that is, the behavior that is defined by the program. The Logic references one of the values that is defined in the AlarmDBObj method (Accept). Referencing a method is referred to as calling a method (see Calling a Method). In this case, the Acknowledge method is applied to the Input1 item when its AlarmState value is Unacknowledged Cleared.
Example: 2
First, we define a database object called 'CDBPoint' which has a method called 'Override' with an LREAL argument (the point override value).
TYPE
AlarmDBOBJ: DATABASE_OBJECT (CDBPoint)
Override: METHOD (LREAL);
END_DATABASE_OBJECT;
END_TYPE
The following ST program block then defines a variable called 'Point' which represents the database point 'Analog Point 1'. The program then overrides this point with a value of 20.0 by using the 'Override' method.
PROGRAM NewStructuredTextProgram
VAR
Point AT %O(Analog Point 1) : AlarmDBOBJ;
END_VAR;
Point.Override (20.0);
END_PROGRAM
Example: 3
This example includes an excerpt from a Logic program that is used to trigger the Tune Limits method. The Database Schema lists the argument data types that apply to the Tune Limits method.
You have to specify the arguments in the method declaration in the Logic program.
To do this, we define a database object called 'CPointAlg' which has a method called 'TuneLimits' with BOOL, LREAL, BOOL, LREAL, BOOL, LREAL, BOOL, LREAL arguments.
(The name that is used for data types varies, depending where you access the value. A Double in the Database Schema equates to LREAL in Logic. For more information, see Data Types for Logic, OPC, and Geo SCADA Expert.)
TYPE
AlarmDBOBJ: DATABASE_OBJECT (CPointAlg)
TuneLimits: METHOD (BOOL,LREAL,BOOL,LREAL,BOOL,LREAL,BOOL,LREAL);
END_DATABASE_OBJECT;
END_TYPE
The following ST program block then defines a variable called 'Point' which represents the database point 'Analog Point 1'. The program then overrides this point with a value of TRUE, 88.0, TRUE, 68.0, FALSE, 0.0, FALSE, 0.0 by using the 'TuneLimits' method.
PROGRAM NewStructuredTextProgram
VAR
Point AT %O(.Analog Point 1) : AlarmDBOBJ;
END_VAR;
Point.TuneLimits (TRUE,88.0,TRUE,68.0,FALSE,0.0,FALSE,0.0);
END_PROGRAM
Further Information
Using Database Object Structures to Access Direct Variables.