GE

Function Name

GE (Greater Than or Equal To)

Description

Outputs a True value when Input 1 is greater than or equal to the other inputs.

Arguments

Input 1 to Input n {ANY}

For more information on the data types for the inputs and outputs, see Data Type Hierarchy.

Returns

Output {BOOL}

The output is True only if Input 1 is greater than or equal to the other input values. If Input 1 is less than any of the other inputs, the GE function outputs a False value.

Example:

Function Block Diagram - GE:

A GE function has 2 inputs (in this case, 2 constant values). Input 1 is has a value of 4 and Input 2 has a value of 2. The GE function outputs a True value as Input 1 is greater than the other inputs.

If Input 2 was changed to have a value of 4, the GE function would output a True value as Input 1 would be equal to Input 2. If Input 2 was changed to 5 instead of 4, the GE function would output a False value as it would not be greater than or equal to Input 2.

ST Program - GE:

The syntax for a GE function in an ST Program is:

Output := GE (Input 1, Input n)


Where Output, Input 1 and Input n are defined as variables earlier in the ST program. Each input is separated by a comma and is a Boolean. The Output value is also a Boolean.

Alternatively, you can use an operator:

Output := (Input 1 >= Input n);


Disclaimer

Geo SCADA Expert 2021