The Logic Tab
The Logic tab appears on the ViewX ribbon when the active window in the Document Display Area comprises a Logic Program.
                 
            
The Logic tab contains the following command groups:
Build
The Build group includes commands that you use when you compile one of the following Logic programs:
- ST Program (see Compiling an ST Program or ST Library)
- Ladder Diagram (see Compiling a Ladder Diagram)
- Function Block Diagram (see Compiling a Function Block Diagram or Function Block Library)
- Sequential Function Chart (see Compiling a Sequential Function Chart).
Debug / Breakpoints
The Debug and Breakpoints groups include commands that you use to:
- Debug an ST Program (see Debugging an ST Program)
- Debugging a Sequential Function Chart.
Library
The Library group includes the Libraries command, which you use to reference an ST Library or Function Block Library (see ST and Function Block Libraries).
View
The View group includes the following commands:
Variables
Displays the Variables window. See the following topics:
Display Settings
Displays the Display Settings dialog (see Configure the Display Settings for Graphical Logic Programs).
Update Interval
Allows you to change how often your Geo SCADA Expert client PC requests updates for a Logic Program. See the following topics:
Connection Values
Displays the current value for the connections on a Ladder Diagram and Function Block Diagram (see Viewing the Values on a Function Block Diagram and Viewing the Values on a Ladder Diagram).