Configuring Lufkin SAMS Digital Input Points

With Geo SCADA Expert’s Lufkin SAMS driver, you use:

The Lufkin SAMS driver supports 1-bit Lufkin SAMS Digital Input points. You configure the properties of each Lufkin SAMS Digital Input point using fields on the Lufkin SAMS Digital Input Point Form.

This section covers configuration of properties on the Digital Point tab of the Lufkin SAMS Digital Input Point Form. For information on the fields on other tabs, see Tabs on Point Forms in the Geo SCADA Expert Guide to Advanced Drivers.

For Lufkin SAMS Digital Input points, use the Digital Point tab to:


Disclaimer

Geo SCADA Expert 2021