Configure the Security Properties

WARNING

POTENTIAL SECURITY BREACH

We strongly recommend using network-connected Geo SCADA Expert drivers in a private network only (either physical or virtual). We recommend against using such drivers for communications over the public Internet. If the drivers are used over the public Internet, as a minimum those drivers should use valid SSL certificates to initiate secure connections and encrypt the data that is transmitted over the network.
Failure to follow these instructions can result in death, serious injury, or equipment damage. The breach in system security could expose sensitive data and the leave the database vulnerable to unauthorized and potentially malicious use.

The Broker tab on the Forms of MQTT Broker items includes a Security section. Use the section to specify whether the data that the broker transmits is encoded using SSL, and if so, to specify the certificate and key settings required for such data transmissions.

NOTICE

LOSS of communication

If Geo SCADA Expert is unable to establish a network connection with a device that uses an SSL certificate, check that the certificate is valid, has not expired, and has not been revoked. Perform these checks in addition to those that you would otherwise perform if Geo SCADA Expert is unable to establish a connection with a device.
Failure to follow these instructions can result in loss of communications between Geo SCADA Expert and the network-connected device.

Disclaimer

Geo SCADA Expert 2021