Enable IO Logging

Associated with: MQTT Broker items

Security permission required to access this pick action: Diagnostics

Used this pick action to enable I/O logging on an MQTT Broker item in the database. When enabled, Geo SCADA Expert logs the communications that occur on the Broker, including any data that is discarded by the driver.

IO Logging on a Broker is not enabled by default. Before enabling such logging, ensure that enough disk space is available to store the log files that will be produced.

Select the Enable IO Logging pick action to display the Enable IO Logging window.

Either:

Select the OK button to enable I/O logging on the MQTT Broker item.

I/O logging on MQTT Broker items works in a similar way to I/O logging on channels on other drivers. For more information, see Enable or Disable I/O Logging on a Channel in the Geo SCADA Expert Guide to Server Administration.

Also see Disable IO Logging.


Disclaimer

Geo SCADA Expert 2021