Create a Mimic on which to Display the Points

  1. Create a new Mimic.
  2. Drag-and-drop the MQTT JSON Schema A Analog Point onto the Mimic.
    A context-sensitive menu is displayed.
  3. Select the Value option.
    A further menu is displayed.
  4. Select Formatted Value option.
  5. Drag-and-drop the second MQTT JSON Schema A Analog Point onto the Mimic.
    A context-sensitive menu is displayed.
  6. Select the Value option.
    A further menu is displayed.
  7. Select Formatted Value option.
  8. Save the Mimic.
  9. Put the Mimic into Run mode.

Once you have configured the Mimic, you can go on to Retrieve Data that is Transmitted by the Broker.

Further Information

Working with Mimics: see the Geo SCADA Expert Guide to Mimics.


Disclaimer

Geo SCADA Expert 2021