Create an Analog Point

Add an MQTT JSON Schema A Analog Point to the database. This type of database item is available from the JSON Schema A sub-branch within the MQTT branch of the Create New menu. The sub-branch corresponds to the message format that Geo SCADA Expert is to use to communicate with the broker.

Geo SCADA Expert will use this point to store the data that it retrieves and processes from one of the analog tags for which the MQTT client publishes data.

When you create the point, you can leave most of the configuration fields at their default values.

On the Analog Point tab of the configuration Form, the only fields that you need to change for this tutorial are:

On the Historic tab:

Save the configuration.

Once you have configured the analog point, you can proceed to Create Another Analog Point.

Further Information

For further information about configuring an MQTT JSON Schema A Analog Point, see Configure MQTT JSON Schema A Analog Points.


Disclaimer

Geo SCADA Expert 2021