Enable Device

Associated with: MQTT JSON Schema A Device items

Security permission required to access this pick action: Disable Points

Use this pick action to place an MQTT JSON Schema A Device item In Service. Triggering the action changes the Device's configuration so that its In Service property is enabled and the Device becomes active.

When the Device item is enabled, Geo SCADA Expert subscribes to the specified topic for which that device publishes data, and receives the messages that the device publishes for that topic. This occurs providing that both the Broker and Device database items are In Service and have valid, saved, configuration, and Geo SCADA Expert is able to connect successfully to the broker.

The Enable Device pick action is only available for an MQTT JSON Schema A Device:

Also see Disable Device.

If using this pick action with the Automation Interface, you need to specify the method name Enable.


Disclaimer

Geo SCADA Expert 2021