Configuring a Map Set

A Map Set is a list of the Map Sources (layers) in a Geo SCADA Expert map. To create a map you combine one or more Map Sources to create a Map Set, which you can then display as a multi-layered composite map. For example, a Map Set could comprise a base layer (such as the OpenStreetMap world map) and a graphic overlay, showing wind speed and direction data. For more information, see Creating a Geo SCADA Expert Map and see Creating a Map Source. 

Each Map Set is represented in the Geo SCADA Expert database by a Map Set database item.

To create a Map Set database item, see Creating a Map Set.

Once you have created a new Map Set item, you need to specify which Map Sources you want in the new Map Set. To do this, right-click on the item to display its Object Menu, then select the Edit Properties option:

Geo SCADA Expert will then display the Map Set form:

This section describes the settings on the Map Set tab of the Map Set form. You can find details of the settings on the other tabs as follows:

Use the Map Set tab to:


Disclaimer

Geo SCADA Expert 2021